Other Parts Discussed in Thread: THS4131, ADS8422, ADS1258
1、THS4131是双电源供电,其单端输入信号范围:-VCC<VIN<+VCC;举例:输入信号是幅值为±4V的正弦波,Gain=1,那么输出的差分信号是:一支是幅值±2V的正弦波,一支是反相±2V的正弦波,这个例子对吗?
2、在一些差分输入adc中,比如ADS8422,有个参数是"absolute input voltag"指出,+IN范围是-0.2<+IN<(Vref+0.2),-IN范围是-0.2<-IN<(Vref+0.2),那说明差分adc的差分输入信号都应该是大于0的,那么因此我在第一条中举的例子就是错的,难道THS413X系列的芯片差分输出是0V以上的反相信号?
3、THS4131有个Vcom脚,这个脚的作用是什么?有或者没有对输出结果有什么影响?
期待您的回复!