Other Parts Discussed in Thread: THS3091
使用THs3091 芯片 放大倍数为3倍 输入为 幅值5V的方波 按设计应该输出15V的方波 可实际的输出是下图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有两点需要注意:
1)THS3091不是轨至轨输出,因此+-15V供电输出并不能达到电源轨+-15V,最高为+-13.2V,因此如果需要得到+-15V 输出,建议再提高供电电压。
2)THS3091是电流反馈运放,反馈电阻的选择很重要,建议采用datasheet中推荐的参考值,在Table4中给出了常见的几种增益,Rf和Rg的电阻值大小,可以参考一下。虽然没有G=3的Rf具体值,但可以在1K~1.21K之间选择一下。