Other Parts Discussed in Thread: OPA211, THS4131
请问OPA可以放大0-1之间的倍数吗?如果这样做会不会导致放大器不稳定?
有没有一款放大器可以在0-1之间放大并且稳定的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA211是一款单位增益稳定的运放,而对于运放增益多大稳定来说,这里的增益指的是噪声增益,噪声增益指的是同相输入,那么可知G=1+Rf/Rg.因此噪声增益不可能小于1. 而对于单位增益稳定的运放来说,实质指的是运放的信号增益小于1. 也就是反相输入的运放,增益G=-Rf/Rg。 因此反相输入,增益小于1,OPA211没问题。
我读出了两点信息:
1、Gain<1,OPA211可以做到稳定;
2、噪声增益是针对同相输入端来说的,反相端没有噪声增益的说法;
3、单位增益稳定的运放都可以做到Gain<1时工作稳定;
-----------------------------------------------------------------------------
我经常在放大器手册上看到“单位增益稳定”,我以为是Gain=1时放大器稳定性最好,那么该怎么理解这个单位增益稳定?
------------------------------------------------------------------------------
除了用类似OPA211的放大器做衰减器外,我还想到了使用差分放大器THS4131作为衰减器,这样可以直接送入差分输入的ADC
一个运放在规定的最小增益上是最不稳定的,OPA211是单位增益稳定的运放,您想放大0-1之间的倍数,可以在信号进入运放之前使用电阻分压器对信号进行衰减,然后让运放工作在规定的最小增益之上,这样就不用担心运放不稳定了。
关于您提到的问题,反相输入的运放同样也有噪声增益这一说,举例来说,Rf=1K,Rg=10Kohm,那么反相输入的G=-0.1, 这个是信号增益,那么噪声增益就是1.1. 并不是说没有噪声增益,但是同样是Rf=1K,Rg=10K的话,同相输入G=1.1 这个信号增益和噪声增益都为1.1. 但这两个稳定性是相同的,因为同样的反馈结构,只是输入操作点不同而已。