Other Parts Discussed in Thread: LMH6629, OPA334, OPA847
我现在想要使用lmh6629型芯片放大幅值为1mV的小信号,但是现在我根据datasheet使用TINA仿真却存在比较大的差异。比较明显的就是芯片手册中可以使用单电源供电但是在TINA仿真中却会导致仿真失败。因此我想请问有没有前辈使用过这种型号的芯片能否给出一个可行的放大1mV信号的电路。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
单电源供电可能就需要注意输入电压范围,需要加合适的偏置才行。不知您是哪里仿真失败,但是这款的Vos为0.8mV左右,所以如果需要放大1mV的信号,尽量选择Vos<<1mV. 比如OPA334,Vos最大5uV。

您好,我现在想做一个能够放大频率100M幅度1mV信号的放大器。不知道您是否有合适的芯片可以推荐,谢谢!
增益要放大多少倍?从而判断运放的GBW至少需要多少albert hao 说:您好,我现在想做一个能够放大频率100M幅度1mV信号的放大器。不知道您是否有合适的芯片可以推荐,谢谢!
那可以看下OPA847,3.9GHz GBW, Vos典型值为0.1mV。