This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2340UA

Other Parts Discussed in Thread: OPA2340

图是电流输出电路,输出电流4-20mA,也可以输出超过20mA的电流,最大到25mAOUT2输出是PWM

测试中发现:

1.校准完成后当电流输出小于20mA,再设置为输出20mA,电流输出正常为20mA

2.当电流输出为22mA或者大于20mA任一值,再输出20mA,用万用表测试输出端输出电流为20.2mA,有的甚至更大。这个现象会不定时出现,有的时候正常,有的时候不正常。

3.在以上1的情况下,用万用表测试R15两端电压时,输出电流由20mA上升0.1~1mA,不同的表上升的不一样。拿开万用表则电流会下降到20mA

4.软件进行了跟踪,在上述12现象中OUT2端的PWM占空比和频率都一样。

以上是我们测试中发现的现象,现象23很奇怪,按理用万用表测电阻两端电压不会影响电路,但是输出电流会变,而且12中的现象像是一种迟滞。

将OPA2340UA换成之前购买的一批没有出现2和3的问题,望解决  谢谢!

  • 亲;PWM频率多大?R26设计错误是导致问题的更本原因。

  • 电路图如附件

    测试中发现:

    1.校准完成后当电流输出小于20mA,再设置为输出20mA,电流输出正常为20mA;

    2.当电流输出为22mA或者大于20mA任一值,再输出20mA,用万用表测试输出端输出电流为20.2mA,有的甚至更大。这个现象会不定时出现,有的时候正常,有的时候不正常。

    3.在以上1的情况下,用万用表测试R15两端电压时,输出电流由20mA上升0.1~1mA,不同的表上升的不一样。拿开万用表则电流会下降到20mA。

    4.软件进行了跟踪,在上述1和2现象中OUT2端的PWM占空比和频率都一样。

    以上是我们测试中发现的现象,现象2和3很奇怪,按理用万用表测电阻两端电压不会影响电路,但是输出电流会变,而且1和2中的现象像是一种迟滞。

    将OPA2340换成别的放大器后,就没有2和3这种现象。

    OK OPA2340问题汇总.doc
  • 之前购买的一批跟现在的是购买地点相同吗?都是从TI授权代理商购买的吗?

  • R26 没有焊接,PWM频率是4KHZ