Other Parts Discussed in Thread: XTR115
图是电流输出电路,输出电流4-20mA,也可以输出超过20mA的电流,最大到25mA。OUT2输出是PWM。
测试中发现:
1.校准完成后当电流输出小于20mA,再设置为输出20mA,电流输出正常为20mA;
2.当电流输出为22mA或者大于20mA任一值,再输出20mA,用万用表测试输出端输出电流为20.2mA,有的甚至更大。这个现象会不定时出现,有的时候正常,有的时候不正常。
3.在以上1的情况下,用万用表测试R15两端电压时,输出电流由20mA上升0.1~1mA,不同的表上升的不一样。拿开万用表则电流会下降到20mA。
4.软件进行了跟踪,在上述1和2现象中OUT2端的PWM占空比和频率都一样。
以上是我们测试中发现的现象,现象2和3很奇怪,按理用万用表测电阻两端电压不会影响电路,但是输出电流会变,而且1和2中的现象像是一种迟滞。
将OPA2340UA换成之前购买的一批没有出现2和3的问题,供货渠道正规,未换过,PWM频率是4KHZ,R26未焊接,望解决 谢谢!