This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR116芯片实现4-20mA电流环电路设计问题

Other Parts Discussed in Thread: XTR116

TI提供了XTR116芯片实现4-20mA电流环电路,但是同一文档中的两个电路图,R2 49.9欧电阻的一端均接了电容,另一端,一个接了地,一个接了IIN

在这里2.2uf电容和49.9欧电阻串联起来后的作用是?49.9欧电阻另一端应该接地还是IIN?

2-wire 4-20mA Transmitter.pdf
  • 看电路这里, 也就是电压基准的滤波电路

    在官方的手册上也有滤波电路, 但是 10 欧姆和电容的滤波.

    如果弄不明白, 尽量参考官方的电路图吧

  • 接地。 更加严谨的是接到Iret(输入电流回流地). 这里的Iret接地,所以49.9ohm和电容是接地的。

    其实这点在datasheet上有介绍,可参考Figure5. 这里RC的作用是为了如果Vref需要接一个容性负载的话,需要加补偿电阻R来保证正常稳定操作。