Other Parts Discussed in Thread: TPA2028D1, TPA2026D2
需要一款音频功放芯片,带扬声器和耳机输出,扬声器输出功率为3W,4欧姆,类似LM3853,但它的功率只有1.5W
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPA2028D1:3 W Into 4 Ω at 5 V (10% THD+N)
TPA2026D2: 3.2 W/Ch Into 4 Ω at 5 V (10% THD+N)
因为您没对供电电压,还有其他电气参数的要求,我举了两个5V供电下的型号。 并且是Class D功放。
如果您还有其他电气特性的要求,可以再讨论。