Other Parts Discussed in Thread: AMC1200
AMC1200输入端测量的是正负75mv的电压,两侧供电为5V,有隔离的
问题1、AMC1200输入端为0,但是仍然在差分输出端有+-1mv的电压,并且,同一款板子,每个差分输出都不一样,有正的也有负的,有部分板子还打到+-2MV
问题2、输入电压在+-0.375MV的时候,光耦的线性度不好,有部分电压,输出端几乎没有变化。
附图为应用的电路,还请TI帮忙看下有什么问题,提下意见
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AMC1200
AMC1200输入端测量的是正负75mv的电压,两侧供电为5V,有隔离的
问题1、AMC1200输入端为0,但是仍然在差分输出端有+-1mv的电压,并且,同一款板子,每个差分输出都不一样,有正的也有负的,有部分板子还打到+-2MV
问题2、输入电压在+-0.375MV的时候,光耦的线性度不好,有部分电压,输出端几乎没有变化。
附图为应用的电路,还请TI帮忙看下有什么问题,提下意见
Hi Beijiang,
问题1:
AMC1200 输入的Offset电压典型值是±0.2mV,最大值是±1.5mV,放大倍数是8,所以典型值经放大之后是±1.6mV,最大值是±12mV。你测得结果在这个范围内属于正常。
问题2:
输入电压±0.375mV,与offset电压相当,且值非常小,所以不容易看出变化。测量线性度应该在全范围内进行测量。
建议参考Demo板,在输入端加共模和差模滤波器。
http://www.ti.com/lit/ug/sbau187a/sbau187a.pdf
看了一下Demo板,输入端的差分是不接到地端的,我们的板子是把输入的其中一条接到地端的。这是否会影响。
问题2里面的线性度的问题,我现在的测量范围是±75MV输入,即发现输入电压±0.375mV这区间线性度不好。
Demo板是差分信号输入,所以没有接地。
如果您一端接GND,是单端输入。