我要放大一个2微伏左右的电压,放大到毫伏,带宽不小于200MHz,有满足要求的运放吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我要放大一个2微伏左右的电压,放大到毫伏,带宽不小于200MHz,有满足要求的运放吗
信号带宽200M还是运放的GBW需要200Mhz?
信号带宽200Mhz的话,那么需要GBW=200M*1000=200Ghz.
如果运放GBW为200Mhz的话,那么有很多高速甚至Ghz带宽的运放,比如LMH6401,带宽到4.5GHz。
如果我信号是从0到100MHz,那么我信号的频率带宽是100M。如果我只放大10倍,GBW=10*100M=1G,是不是我需要一个GHz带宽的运放?我还想请教一个问题,我想放大一个微伏的信号,各种干扰信号都可能比他大,这个能实现吗?运放能把他放大出来吗,是不是运放的噪声足够小就可以?
亲;这个课题可能已经超出了绝大多数工程师的能力,建议考虑成熟后再动手。
关于你的课题,建议分成三大块:前级:高频放大和低频&直流放大。最后用加法混合平衡后末级放大。
建议高频与低频/直流的分频点建议设置在1M。1-200MHz频段设为高频段,0-1M做低频段。
高频段建议用GaAs超低噪音双栅场效应管做前级放大。共三级电容耦合串联,每级放大10倍。共1000倍。可用管子:3SK240等。这是参考资料链接:http://www.doc88.com/p-9813441718341.html
低频段建议用两颗OPA2189,分别接成5.6倍比例放大器,共4级;串联,成为1000倍前级放大器。
高频输出和低频输出混合相加,配平增益和相位后,用OPA2836-Q1或THS4541-Q1做单位增益缓冲输出。