您好,我用LM2903做比较器来控制对管输出功率信号,附件是相应功能电路图,待机时PWM地方为低电平,电阻R66上端输出为+12V信号,现在丝印为75A批次的LM2903(U17)7脚输出为9.9V以下,造成电阻R66上端输出为+10V以下;其它丝印的LM2903(U17)7脚输出为11V以上,电阻R66上端输出为+12V。现在想知道是什么原因导致。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为这是一款open drain的输出,所以输出低电平取决于输出端上拉的电平。
换句话说,您的意思是丝印75A的输出不正常,那么您两个不同丝印的LM2903 的购货渠道一致吗?都是通过TI授权代理商购买的吗?
你好,购货渠道我再找我们sales确认,请问这个设计图是正确的吗,比较器输出低电平时0V,是不是上面的PNP管和下面的NMOS都满足了导通的条件?
PNP导通的条件Ueb>Uce即可导通。同样,NMOS导通条件,Ugs>Uds即可导通。
如果LM2903输出低电平的话,上面PNP和NMOS都是导通的,
但实际上,LM2903是OD输出,输出低电平取决的上拉电压值的大小,所以LM2903的输出也是高电平12V,这样的话,上面PNP是截止的,下面NMOS是导通的。 R66输出应该是负压,我用同样是OD输出的LM293 简单仿真了下,结果相同。 您可以看下。
你好,还有不懂的就是,LM2903输出低电平时您说上拉也是高电平,那LM2903输出高电平那肯定也是12V电平,这个电路还怎么输出低电平呢,另外我看LM2903的IOL Low-level output current是6mA,是不是意味着低电平输出时有6mA的灌流能力,如果是,R62和R63并联后再3.75K阻值,乘以6mA等于2.25V,12V-2.25=9.75,既表明这个电路有问题呢?确实有疑惑,如有理解偏差比较大,还请包涵。