Other Parts Discussed in Thread: TL431
该运算放大器采用5V单电源供电,其输出端和反相输入端直接连在一起做电压跟随,运放上电后,同相输入端输入2.49V的参考电压,一开始运放跟随输出2.49V的电压。可是用了一段时间输出板变成了0.7855V,又过了一段时间,输出又变为2.49V,想知道运放做电压跟随为什么会出现这样的情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TL431
该运算放大器采用5V单电源供电,其输出端和反相输入端直接连在一起做电压跟随,运放上电后,同相输入端输入2.49V的参考电压,一开始运放跟随输出2.49V的电压。可是用了一段时间输出板变成了0.7855V,又过了一段时间,输出又变为2.49V,想知道运放做电压跟随为什么会出现这样的情况?
我测量了一下,这个芯片输出和它的地之间,测量电阻稳定后是123K左右
正常情况下,Gain=1,闭环输出阻抗为200ohm。
建议更换芯片再试试,看是否都是类似情况,工作一段时间异常情况。
不是输出阻抗引起的,我这里所说的200ohm,测试条件是在3V供电,f=7KHz,Gain=1. 并且datasheet中也给出了输出阻抗和不同频率之间的曲线。
如果您的电路是跟随器的话,直接接输出跟随输入,输出阻抗增加也是可能的,这也通常是提到输出阻抗的解决方法。
就您目前跟随器输出不稳定的情况来看,如果不是焊接,带载问题的话,很可能就是器件本身的问题。