This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
呃呃,是这样的。检测部分好弄,然后主要是为了隔离这个信号。 我按这个电路测试时,I=4ma时,Vout在2v附近,不是应该Vin=Vout=0.4v吗
ISO124输入输出范围离电源轨较远,两端都用±5V供电试试
ISO124的供电电压范围为+-4.5V~+-18V,也就是说单电源供电最小为9V。
另外,ISO124的offset比较大,+-50mV最大,所以直接采用100ohm Rshunt分压对电流采样,可能会造成误差比较大。
或者建议采用datasheet 9.2.5 Isolated 4- to 20-mA Instrument Loop的方案,先使用4~20mA receiver RCV420输出电压信号,再使用ISO124 进行隔离。
板子提供不了这么高电压。。。然后想换个方案。。vf→光隔→vf不知道行不行?对于4-20ma隔离你还有更好的方案吗?板子现在能够提供5v隔离电压。。