通电后,负压-5V正常,一旦INA163有信号输入,LM2662马上就坏了,负压输出只有-0.29V,重新上电也是这样。芯片也不烫,连续两块都是这样。
请问问题出在哪里?INA163的使用电压下限是正负4.5V,在正常工作范围内呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM2662给INA163 供电没问题。
检查下焊接是否有短路地方。或者给INA163单电源供电,给输入信号看INA163是否正常工作。
短路没有。我把INA163的PIN6负电源接地,正电源接+5V,输入一个幅度0.5V频率500Hz的差分信号,放大倍数是7,输出始终是1V左右的直流电平,换了个INA163还是这样。