Other Parts Discussed in Thread: OPA2369, TINA-TI, OPA2313
opa2369对2.5V和1.2V进行电压跟随,2.5V很稳定,但1.2V产生震荡。输入端接了小电阻隔离,但仍然震荡,只不过震荡比没接小电阻隔离小一点。怎么搞?难道这非单位增益稳定运放真不能用作电压跟随?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi JIANG GUOYUAN,
应该是电路稳定性出问题了。
用TINA-TI仿真得到电路的相角裕度为-70°,处于不稳定状态,所以会震荡。
这是由OPA2369带容性负载造成的。OPA2369的开环输出阻抗非常大且呈感性,外部带10nF负载也非常大,两者相互作用形成的双极点频率较低,在2kHz左右;添加的隔离电阻R16,R258阻值太小,阻尼过小,对系统矫正作用微弱。
有两条建议:
1. 增大隔离电阻至20k-50k左右,或者降低输出滤波电容;
2. 换成输出阻抗较小且呈阻性的运放,一般Bipolar的运放输出阻抗呈阻性,CMOS的输出阻抗变化稍大。OPA2xx多为Bipolar运放。
Hi Willing,
thank you for your reply.
我接下来做了如下尝试,R258换成50K,仍然震荡,在这基础上,去掉C203的电容,仍然震荡。
但接下来当我把R258提高到1M的时候,震荡消除,但此时波形不是特别完美,杂波比较大。但基本能用。
我还有如下问题需要请教:
1. 为什么2.5V的基准电压经过opa2369的电压跟随之后,不会发生震荡,但1.2V很明显;
2. 附件中是Ti 另外一个关于电压跟随自激震荡的帖子。website: https://e2echina.ti.com/question_answer/analog/data_converters/f/58/t/48350 ,
我将其中一个电路截图到下面,请能解释这个能消除自激的原理,
Hi JIANG GUOYUAN,
有几个问题和建议:
1. R257, R259这两个电阻在测试的时候焊接了嘛?如果焊接了则将稳压管直接连接到输出端了
2. 可以把两路的输入输出波形发一下吗?每一路的输入和输出在一张图片上
3. 系统的电源又是怎样的呢?建议用LDO供电。
4. 可以做了个交叉实验,将2.5V稳压管换成1.2V看是否震荡;如果不震荡,那表明电路设计可行,问题在于1.2V的布板;如果震荡,则表明电路原理设计存在问题。
Hi Willing,
关于这个问题 , 我现在查找下来,应该是我1.2V后面有太多的电容负载。我这个1.2V后面接了30路到opa2369的正输入,所以输入电容很大。但我的2.5V电压 ,后面只是作为分压源,后端没有接什么元器件。因此1.2V震荡而2.5V不震荡。看来暂时方法也只有加大的隔离电阻了,由于后端的输入电容大小也不确定,只能一个电阻慢慢调试。现在大概增加到500K的时候,基本上震荡消失了