This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐性价比合适的跨阻放大器

Other Parts Discussed in Thread: OPA354

我们要设计一款低速(DC-2Mbps)的可见光(520nm)接收器,目前选择了两种光敏管,其参数分别如下:

光敏管1参数:反向电压16V,Tr,Tf=90ns,结电容(VR= 0 V, f = 1 MHz, E = 0)135pF

光敏管2参数:反向电压50V,Tr=10ns,结电容(VR= 0 V, f = 1 kHz, E = 0)6pF

求推荐性价比合适的跨阻放大器。谢谢。