Other Parts Discussed in Thread: LM6134, TL974
LM6134太贵,想换个PIN TO PIN的, 用了TL974但是不工作, TL974只能双电源吗? 哪个可以替代?麻烦推荐下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,单看12V供电的话,二者是都可以的,但是还要看其他指标。就TL974来看,它的共模电压范围为(V-)+4~V+,也就是说如果您单电源供电,那么输入信号的幅值最小为4V。 所以200mV输入信号没在其共模电压范围之内。
而LM6134是轨至轨输入输出的运放,也就是说输入输出都能达到电源轨,所以200mV输入是没问题的。
所以您可以验证下TL974,给它一个满足输入范围的信号,看其是否正常工作。