Other Parts Discussed in Thread: INA333
请教专家:
INA333在单电源工作时,数据表建议REF接VCC/2。如果输入信号是正的,是否偏置可以偏置为1V或更小?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
kailyn Chen:
谢谢!继续请教!
我在用Pt1000做温度采集,采用INA333做放大,见附图,REF偏置调为4V。PTR+\PTR-之间接入Pt1000,调整R35+R36=1.0390K,在Pt1000=1.0390K时(对应温度10°C),超出10°C时,Pt1000的阻值大于1.0390K,反相端的输入大于同相端输入。Pt1000=1.0390k时,INA333输出为4V。在Pt1000=1.4795k时,想调整输出接近INA333的下轨输出,问题是:无论怎样调整INA333的增益电阻,调整R32、R34(考虑饱和问题,加大这两个阻值), 都不能接近下轨输出,最好的情况是,增益电阻为2k、R32=R34=2K,INA333的输出是1.2V。请指教!