大功率功放电路发热严重,不知什么原因!有原理图和实物图
电路如下图,用opa445+opa549
输入一个正弦信号,输出接一个5W的小喇叭,就烫的不行。这功放可是10A呐 这也就才1A多
而且有个特别奇怪的现象 下图是电源
输入交流18V 不知道为啥opa445发热特别厉害,这是个前级运放咋还发热?
但是我用7812和7912直流正负12V输入的时候测试,opa445不热,opa549还是依然那么热,LDO都没那么热,一个功放那么热,那要是到满功率······
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.