This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于RCV420芯片的信号输入问题

Other Parts Discussed in Thread: RCV420

你好,RCV420芯片是比较经典的测量4-20mA电流信号的芯片,可是仍然是DIP封装,尺寸较大,一块板子需要24路信号测量还是很浪费空间的,请问有没有更小的封装?或者其余的芯片可以替代?

该芯片低温工作温度是否能到-25摄氏度?

另外,请问外部两线的4-20mA信号输入时,是否可以将电流信号接入3脚,外部地与芯片地连接,芯片1脚悬空2,2脚接地?

芯片8脚悬空是否可以?

  • 1.首先我们只有这一款4~20mA 接收器,目前还没有替代品,如果需要找替代的话,可能就需要用分立器件去搭建,比如使用仪表运放去构建。
    2. RCV420的温度范围,datasheet中有给出,Specification 范围为0~70度。operating 范围为-25~85. 这二者的区别在于在Specification范围内使用性能最佳,而超过这个范围,在operating范围内的话RCV420仍能正常工作,但有可能会性能降低。
  • 另外,输入电流可以经过3脚,然后2脚接地给一个回流路径,1悬空即可。
    如果不需要reference trim的话,8也是可以悬空的,如果需要的话,可参考datasheet Figure7的电路Optional Voltage Reference External Trim Circuit.
  • 非常感谢详细解答,我目前是按datasheet的FIGURE 1. Basic Power Supply and Signal Connections设计的,用于测量4-20mA电流信号,正负12V供电,不知道能不能成功?