你好,TI的工程师,目前正在做一个高精度的4~20mA电流测量设备,有一些疑问:
(1)请问一个+28V驱动的4~20mA电流信号,RCV420芯片能否直接接收?
(2)芯片的共模输入范围为±40V,是否意味着电流信号可以由-40V~+40V之间的电压驱动?
(3)芯片输出的0-5V与输入的4-20mA电流之间是否是线性(成正比)关系?
(4)芯片的输出端加一个ISO122/ISO124是否会影响测量精度?
(5)ISO122性能好还是ISO124性能好?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.