This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

仪表运放用作电流检测的疑问

Other Parts Discussed in Thread: INA826

INA826的datasheet上有一个低端电流检测电路,仿照这个电路在TINA上搭建了一个高端电流检测,用一个5V电压源,输出给一个1 ohm 采样电阻,然后加一个500欧负载电阻到地,INA826接采样电阻的两端,放大100倍,输出电压是-200uV。

把这个电路改成低端电流检测,把采样电阻和负载电阻交换位置,就可以了,输出达到了预期的1V。

问题是,INA826这个仪表运放,在这里为什么只能检测低端电流,不能检测高端电流?

在电源论坛里问过了,有个大神说是直流偏置问题,但是没有详细讲解一下,这里有没有运放老司机帮忙解答一下?

  • 高端接测,我们知道Rshunt是放在VBus和Rload之间,因此共模电压就是要监测的Vbus电压,这就要求运放的共模电压一定要达到电源轨才行,而INA826的共模电压最大要在(V+)-1V之内,所以达不到电源轨,而低端检测的共模电压实际为0, INA826的共模电压包含了负压轨,所以是可以用来做低端电流检测的。
  • 把INA826的电源设置成正负15V重新仿真了一下,你说是对的。我对钻石图还不是很理解,我再找找资料学习一下,谢谢!