This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA139带宽问题

Other Parts Discussed in Thread: INA139, TPS53632G

TI的专家:

最近使用TI的TPS53632G芯片设计了一款电源,开关频率1MHz。电流采样使用了INA139,看数据手册上当负载电阻为1K的时候,带宽可以到1M,可是目前应用在1M的开关频率上有问题,INA139的负载电阻配置为1k电阻并联10p电容。将频率降低到500K,这个时候电源就正常了。判断是电流采样有问题。INA139可以用到1M的频率或者更高吗?如果不可以,有没有其他的高端采样且输入共模电压与供电VCC独立的芯片?

  • 首先, 我觉得数据手册给出的数据是可信的. 但是应用到实际电路就不一定了, 因为有电路里各自因素的影响.
    所以你的问题可能是普遍问题, 增加设计裕量是个办法
  • 亲;用1M带宽测1M噪音信号,本身是极风险的。带宽1M是指1M时异样45度。这也意味着占空比一旦超过50%就有次谐波振荡的风险。
    通常;电流检测带宽要么按LC滤波常熟选取;要么至少达到开关频率6.28倍。
    关于带宽问题;建议给出原理;看看你的用法。无电路无真相,对电流检测运放也就没得建议了。