This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm331 F to V 元器件推荐

Other Parts Discussed in Thread: LM331, LM321, OPA320, LMP7721

你好,TI

用LM331做了一个样机(频率转电压),初步可以达到目标。pdf的Figure 19,图纸上电压输出部分有个运放,可以推荐下型号和大概接法吗。

本来计划使用LM321做反相接入的,结果不行(电压被拉低,输出异常)。

请推荐一款平价/好买的运放(封装尺寸不要太小,不便焊接。最好是SOT/SOP之类的)。

  • LM331 是电流输出,所以要想转换为电压Vout,输出端接了个运放实现I  to V的转换,

    运放的选择主要考虑Iib要尽量小的精度运放,或者跨阻运放,Vout=Iout*Rf

    比如OPA320, LMP7721等这类精度运放,另外需要注意您需要实现多大电压的输出,像您说的LM321 输出被拉低是不是因为输出饱和导致/

  • 输入5-15K HZ,50%占空比方波,幅值12V。
    输出DC 1.25V-3.75V。

    能不能多推荐几个合适的运放,因为涉及到成本,需要尽量挑性价比高的。。


    目前LM331供电15V测试还算行。但是这个15V并不是非常理想,故准备改用5V供电。

  • 你好,我注意到LM331pdf里面的这个运放是有负电源供电的。

    我现在板子上只想给出5V供电。(负电源太麻烦了)

    如果采用OPA320参与设计的话,能不能满足我的设计要求。(OPA320里面好像并没有强调负电源供电)

    设计最好简单点,不要太复杂。