Other Parts Discussed in Thread: LM331
你好,各位老师。
设计指标:输入5-15KHz,幅值12V,占空比50%的方波。
输出1.25V-3.75V(对应频率)。
经过proteus仿真和PCB上电测试,样机在供电15V时没有问题。
现在供电需要改成5V,proteus仿真输出没有问题。但是实际上电输入15Khz时,输出电压输出只有3.64V。(后续频率如果继续调高,最高也只有3.64V)
5KHz-14KHz时,电压转换都正常。
这里是不是有个范围限制的?(参考文档在figure1&2)snoa734b.pdf