This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
刚开始选的INA122,带宽太低了
http://www.ti.com/paramsearch/docs/parametricsearch.tsp?family=analog&familyId=1612&uiTemplateId=NODE_STRY_PGE_T
可以选用以上选型工具,更具您的需求进行选择。
谢谢
楼主你好!
请帮忙确认两个问题:
1、能否给出具体应用信息?
2、输入信号范围、信号源阻抗、信号频率成分?
1 应用于热电偶的第一级放大四十倍左右
2 K型热电偶输出满量程大概50mv,阻抗大概10欧作于,信号平率最高100K
我选择了INA155或者156,您看合适么?还有一个关于INA155、156的问题在这儿http://www.deyisupport.com/question_answer/f/52/t/17622.aspx
INA155 INA156可以满足楼主应用的带宽要求。
FREQUENCY RESPONSE
Bandwidth, –3dB
BW G = 10 550 kHz G = 50 110 kHz