能否提供一种设计方案能满足如下要求:(1)信号的带宽为1.5MHz~5.5MHz;(2)信号源的阻抗为120欧;(3)信号源的幅度为10uV左右,要求在3.5MHz左右实现100dB左右的增益,把信号放大到几百mV左右。在这么宽的带宽以及高增益的条件下,如何实现低噪声要求。要能正确输出10uv放大后的有用信号而不被噪声或干扰淹没。请提供解决方案,谢谢!我之前采用LMH6629和OPA659组成三级运放,但是发现即使输入不接信号源,三级放大后输出都有几十mv的噪声或者80MHz左右的正弦波。请问这是什么原因导致的?