Other Parts Discussed in Thread: NE5532, TPA3245
按照官网给的原理图画板安装之后,A和B通道输出正常,C和D通道在放大声音后,低音出来的时候喇叭突出很明显,声音也是异常的,如果输入和输出A通道和C通道,两边声音都是异常,只有在BTL模式下A和B、C和D输出没有问题,请问这个问题怎么解决?项目进行中,请TI工程师看到信息后及时回复,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
1,输入音频信号为普通模拟信号;
2,信号输入INPUT_A对地为一组、INPUT_B对地为一组、INPUT_C对地为一组、INPUT_D对地为一组,共四组信号输入;
3,信号输入直接输入到2个NE5532,运放的输出信号分别输入到INPUT_A、INPUT_B、INPUT_C、INPUT_D到TPA3245这四个通道(这个电路是参照官网提供图纸所画PCB板);
4,输出信号每一组都经过红色发烧电感后再经过50v1500uf电解电容输出接喇叭正极,负极接地,每一组都是一样的;(电解电容试过更换50v470uf故障一样);
5,试过把M1和M2的的引脚按照图27接法,在输入单个信号时(独立输入L信号),A和B两个通道同时都有输出,把M1和M2的的引脚接入地后通道独立工作正常;
现在这样描述可以看清楚信号流程吧?故障还是前面所描述现象,你们的实验板有实验过单通道输出吗?是否工作正常?