This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于高速运放的选择

Other Parts Discussed in Thread: LMH6624, OPA838

我现在想把一个频率为几十MHz,幅值为几十mv的信号放大十倍,请问有没有什么常用的性价比比较高的运放推荐啊?

  • 您好,
    感谢您对TI产品的关注!
    您可以看下LMH6624,工作电压范围±2.25V ~ ±6.3V,输入失调电压 (limit over temp) 700 µV,如果您给我具体的最大输入信号带宽和输入信号最大幅值,我可以再帮您筛选下型号
  • 输入信号最大频率为25MHz,幅值无法确定,但是有一个大概的范围,最大幅值大概就是几十mv,不超过100mv。还有什么型号可以推荐的吗?
  • 输入信号最大频率为25MHz,放大10倍,要求GBW最低为250MHZ,您可以看下OPA838,GBW:300MHz
    单电源工作电压范围:2.7V 至 5.4V
    25°C 下的输入失调电压:±125µV(最大值)
    OPA838虽然是轨至轨输出,但注意输出不能完全达到电源轨,如果输出有在100mV以内,请使用双电源供电