大家好,我使用PGA281做程控放大,G4设为低电平,G3-G0改变参数,EF输出正常,但输出信号放大倍数没变化,始终在十倍左右,原因是什么?调整输入信号幅度和频率,输出信号也随之相应变化,就是调整不了放大倍数。VSP-VSN=24V,VSOP-VSON=5V,VDD=3.3V,VSON=-2.5V,VOCM串一个2K电阻接地。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我使用PGA281做程控放大,G4设为低电平,G3-G0改变参数,EF输出正常,但输出信号放大倍数没变化,始终在十倍左右,原因是什么?调整输入信号幅度和频率,输出信号也随之相应变化,就是调整不了放大倍数。VSP-VSN=24V,VSOP-VSON=5V,VDD=3.3V,VSON=-2.5V,VOCM串一个2K电阻接地。
您好,VSON的电压范围是(VSN)~【(VSP)-5V】。
也就是说,如果+-12V供电,VSP=12V, VSN=-12V,VSON的电压范围为-12V~7V。 所以VSON接-2.5V是没问题的。
另外Vocm的电压范围为(VSON) + 0.1V~(VSOP) - 0.1V. 所以如果VSON接-2.5V的话,那么Vocm接GND是在这个范围之内的,也没问题。
那还得打扰下,我用的是标准电路,为什么这么接放大倍数不可调,固定在10倍左右,换了一片芯片也是这个问题。后来vson改成接地,vocm接2.5v. Vsop接5V就正常放大,倍数可调