Part Number: XTR115
R25/26输入端电压1V ,输出端电压1.1V 电流输出10.1mA请教下这个0.1V的偏差如何避免
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在两线制变送器中,XTR115前级电路的供电都需要从24V端电源供电,且整个系统的功耗必须小于4mA,具体查看:
e2e.ti.com/.../part-2-two-wire-4-20-ma-transmitters-background-and-common-issues