This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1211-Q1: 采样电压范围的问题

Part Number: AMC1211-Q1
Other Parts Discussed in Thread: TLV313,

您好

我的这个电路我最终的TLV313输出的电压最大就是2.4V,输入电压大约大于2.4V时,输出电压就不随输入电压增大而增大了,这是为什么?对此我有了一定的理解,您帮我看一下对不对,如果不对,麻烦您更正一下。

我看了datasheet有个参数时VCMOUT=1.44V,这个意思是:OUTP=VCMOUT+VIN/2,OUTPN=VCMOUT-VIN/2(指的是对GND2的电压),datasheet中6.1表中说出了OUTP,OUTN的电压范围,最小是GND2-0.5,最大是VDD2+0.5,我的电路图中VDD2是5V,实际上4.7V(VDD2由14030供电由于没找到合适的FB电阻但一定是大于4.5V的,),通过6.1中说的范围我的理解是输入电压VIN最大是2[VCMOUT-(GND2-0.5)],也就是2(1.44+0.5)=3.9V,所以我的理解是这个芯片的有效采样范围是0-3.9V,所以有两个问题。

问题1:如果我的理解正确,为什么我实际测量有效采样范围是2.4V,是哪里出了问题吗?

问题2:有更宽的采样电压范围的型号吗?我想要用MCU采极单端输入0-5V,有推荐的型号吗?

  • 您好,

    下面是AMC1211-Q1 datasheet截图,可以知道,其线性输入范围是-0.1V~2V,超过这个范围就不再是线性输出;

    VCMOUT是AMC1211-Q1的共模输出电压典型值,VCMOUT=(OUTP+OUTN)/2,AMC1211-Q1具体您可以看datasheet Figure 44. AMC1211A-Q1 Output Behavior

    TI满足0~5V输入范围的隔离放大器有下面5个,没有汽车标准的