This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9044: 功耗随信号频率变化,正常吗

Part Number: TLV9044


手册上描述静态10ua/通道,我在使用过程种发现功耗随信号频率增大而增大,频率450HZ的是已经到250ua左右,这个芯片就是这样还是使用上有什么特殊的地方我没有注意到呢

  • 您好,功耗是静态功耗和输出功耗两部分和。静态功耗指的是没有输入信号的前提下,流经VCC的电流。

    输出功耗是和负载有关的,或者和输出电压有关的,datasheet中FIgure7-15和7-16给出了output voltage VS output current的关系。

    您这里提到和频率有关,是只改变了输入信号的频率? 由于压摆率的影响,SR=2*PAI*Vo*f。 随着频率的增加,那么最大输出电压是降低的,输出电压降低,输出电流是增大的。所所以您看下当随着频率增加的时候,输出是否变小?