This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA567: 仿照手册里的Howland恒流源电路做了一个驱动电路,但是焊接之后没反应,求求大佬救救萌新

Part Number: OPA567
Other Parts Discussed in Thread: TLC2252

电路图设计如下:

ENABLE引脚和IN+引脚都给了5V输入,但是输出为0,枯了枯了,调了一天也没调出来是什么问题,救救萌新吧orz

  • 我测出来实际电路供电没有问题,IN+输入0.1V,和仿真不同的是TFLAG和IFLAG,仿真中TFLAG=5.0V,IFLAG=5V,但是实际电路中TFLAG和IFLAG都为0V,但是我这温度和输出电流明显都没超标,是运放没工作,还是运放是坏的哦?跪求大佬!!!

    仿真电路如下:

  • 您好,

    我用TINA 仿真也是没问题的,如下截图:

    建议先去掉TLC2252电压跟随器,或者验证TLC2252电压跟随器是正确工作的。

    然后检查下焊接问题,或多测几款板子看输出情况?

    如果怀疑运放已损坏,可以拆掉换新的芯片以验证输出