Part Number: INA302
Other Parts Discussed in Thread: INA208, INA205, INA201
大家好,
我现在有一个模拟输出模块需要做过流保护,模拟输出模块的电压是±12V,需要检测这个输出模块(实际上是一个放大器)的输出电流,当输入输出电流超过±20mA时,给出报警信号。我看INA302的内部功能基本上是够的(包含检流放大和门限比较),就是检测电源只能是正电源,不能检测负电源。想知道有没有其他现成的IC可以满足我的要求?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,可以参考下INA20x系列电流感应放大器,比如INA205,INA208,它的共模电压范围为-16V~80V的宽电压范围,也是内部集成了比较器。
但是和INA302的不同之处在于,INA302可以调节电流限制的门限电平,有ALert引脚,而INA20x系列的没有,他们限制电流的方法是根据比较器的输入电压以及内部电阻,参考下面比较器的内部结构。所以可以看到,电流限制在1mA范围之内,所以可能无法满足您的要求。

带有比较器的电流感应放大器基本上是INA20x和INA30x系列,但是INA30x系列的共模电压范围是正电压。
所以如果如果输出模块是+-12V的话,是否可以考虑加个偏置电压,将其电压抬高到正电压,再给INA302 输入。
您好,集成单个比较器的,可以看下INA201,共模电压范围为-16V~80V, 高边电流检测的一款电流感应放大器: