Part Number: AMC3301
各位前辈们,我在做一个基于电阻分压的检测电路,正常检测时候输入端输入的是60V左右的直流电压,但是会存在过电压冲击,使得用于采样的分压电阻上面也会因此产生峰值1000V的电压,对于后端电路会产生破坏,现在想用TI的这款隔离放大器,但是不确定一个问题:当隔离放大器的输入超过规定的范围(±250毫伏),输出会是多少,等于电源电压吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
AMC3301输出模拟电压特性如下数据表截图所示,对于-250 mV至+250 mV范围内的差分输入电压(VINP–VINN),该设备提供了标称增益为8.2的线性响应。例如,对于250 mV的差分输入电压,差分输出电压(VOUTP–VOUTN)为2.05 V。在零输入(INP对INN短路)下,两个引脚输出相同的共模输出电压VCMout,如电气特性表中所规定。对于大于250 mV但小于320 mV的绝对差分输入电压,差分输出电压的幅度继续增加,但线性性能降低。如果差分输入电压超过VClipping=±320mV值,输出在VCLIPout=±2.49V的差分输出电压下饱和,如所示图 7-2。