Other Parts Discussed in Thread: OPA210
各位老师好:
1:以上电路连接能否实现0-10V直流信号输出?
2:单电源运放必须要1/2 VCC偏置吗?
3:什么时候用直流耦合输入,什么时候用交流耦合输入?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,首先OPA2210的输入电压范围(V-)+1.5V~(V+)-1.5V。所以如果单电源供电,输入信号最小电压为1.5V,12V单电源供电,输入信号的范围为1.5V~10.5V。
2.单电源供电,加偏置的目的就像上面我说的,因为最低1.5V输入,那么0~1.5V的信号无法处理,所以如果加了偏置电压,使得输入信号的电压被抬升到满足输入电压范围之内,这样就能正常工作了。
3. DC和AC耦合的主要区别在于,AC耦合改变了输入信号的共模电压(电容隔直),由于输入信号的共模电压不满足芯片输入共模电压需求,所以需要在输入端重新建立新的共模电压。如果满足的话,可直接DC耦合接到输入端。
您好,按照您的电路,Gain=1+R2/R1,R 1=R 2=100K,所以Gain=2,即为3~10V的输出。
另外需要注意的是,如果您只是用一路的话,可以直接使用单通道的OPA210。 2210是双通道的,不用的通道也不建议输入端悬空处理,最好是搭成单位增益。