This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA551: 帮忙解释典型应用说明

Part Number: OPA551

下图是OPA551手册中的一个典型应用,请帮忙说明note的内容和我的疑问:

1. 图中R3如何限制电流?我个人认为去掉R3更好,因为R3会导致输出误接高电压时损坏运放,如果没有R3,高压只可能损坏两个三极管。

2. 允许在输出-0.7V~0.7V运放驱动负载,如何理解?我使用仿真软件,输出0.4V,1A时,负载电流主要还是通过三极管提供,100Ω电阻的电流很小。

3. 图中CF作用是什么?如何确定容值?

4. 图中0.2Ω电阻作用是什么?如果想更改功率更大的三极管,此电阻如何选择?

图下的NOTE内容是:1. R3提供电流限制;2. 当输出是-0.7V~0.7V时,运放驱动负载。

  • 您好,

    1、R3主要是通过流经其上面的电流,然后产生0.7V压降来偏置三极管使其导通用的。去掉R3后,三极管无法导通。

    2、如果没有R3就没有R3产生的0.7V压降,在运放输出小于0.7V时,后面三极管无法导通,就无法通过三极管给负载提供电流。

    3、如果反馈电阻与运放输入电容(加上一些杂散电容)形成较大延迟,会使放大器不稳定或者输出出现过冲和振铃,在电路中加上CF可以解决这种现象,CF的选值是CF*RF=Cin*RG通过这个式子来计算,RF是反馈电阻,Cin是输入电容(包括杂散电容等各种输入电容),RG是增益电阻。由于杂散电容存在不确定性,因此也无法确定出CF具体大小,一般通过实验测试调节来确定具体值。

    4、0.2Ω应该是起到负载短路保护的作用,这个可根据实际应用来设定。

  • 1和2. 我昨天通过仿真,在取消R3时,同样的输入0.2V时输出0.4V,输出是正常的。请帮忙解释。我的理解是只要运放负反馈正常时,运放输出会控制三极管状态,给三极管提供Ib电流,电流进而决定了导通电压。

    3. CF没有一个大概的计算公式吗?

    4.  我没有其他问题。

  • 1、可能您使用的三极管导通压降不到0.7V,或者小于0.4V,如果三极管BE没有正偏,它是不会导通的。

    2、CF的大概计算公式就是CF*RF=Cin*RG,只有您能确定Cin就可以,关键是Cin不易确定,因受杂散电容的影响,您可以先根据运放的输入电容值计算出的CF值开始尝试调节。