Other Parts Discussed in Thread: TL072, TL072M, TL072H
用TL072来搭建比较器输出,反相输入端是9.3V电压,同相输入端是0.3V,但是输出电压确是高电平输出,同相端输入变成2.5V后,输出电压是0电平,符合要求,请问是怎么回事,做比较器的时候,不是同相输入大于反相输入就输出低电平,同相输入小于反相输入的时候就输出高电平吗,那第一种情况是怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,不知您使用的TL072哪款,因为TL072有TL072H, TL072M等一系列后缀,但是它们都不是轨至轨输入,可以看下面电气表格,TL072H 的输入电压最低(V-)+2,比如12V单电源供电,至少2V输入才行,同样TL072M或者TL072I系列的,可以看到输入共模电压最低(V-)+4V,也就是单电源供电的话,至少4V输入。 所以对于接近0V的信号是无法处理的,所以如果信号靠近0V,建议改为双电源供电,就没问题了。