现在用的ADS1118,单电源供电就可以测量热电偶的负电压信号,但是ADS1118最多放大16倍,我们热电偶最多检测100度(还需要测量比室温低的电压,所以有时输入负电压),这样AD位数就浪费了,有没有一款放大器能放大到500或1000倍的,单电源供电可检测负电压的放大器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在使用的是T型热电偶,热电偶响应率约为40uV/度,静态下测试了一下精度还可以,就是觉得16AD位浪费了6位。热电偶信号前端有射频信号影响,把放大倍数提高精度是不是能提高测量精度、且抗干扰能力提高呢?
楼主你好!
1、对于射频干扰,由于射频信号频率(高频信号通常大于100khz)和热电偶信号(低频或者是直流信号)不属于同一频段。可以使用RF filter,在ADC/PGA 或者 INA 前增加滤波器,可以用分立的R C做,也可以用集成的RF filter(murata有供应)。
2、增加放大倍数会提高信噪比,但是对于射频干扰,主要通过RF filter滤除。