Part Number: OPA858

我使用这种电路时,无输出,会是什么原因。求帮助
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,OPA858的第8pin是PD引脚,低有效,PD=L的话,输出disable,OPA858进入低功耗状态,所以看下这个引脚是否拉低了。
另外,这是一个微电流放大的电路,Vout=Iin*Rf. 如果PD没问题,检查下各个引脚焊接,供电电压是否正常?
或者搭建一个简单的同相或反相电路,看下是否有输出?注意OPA858是Gain>=7时稳定。
MPPC的结电容是42pF的,对稳定性的影响大吗?另外MPPC是直接连OPA858的反相吗 需要串个电阻不?
您好,MPPC的结电容越大,那么OPA858的-3dB的带宽越小。计算公式如下,我们可以通过这个公式计算下稳定带宽大约为多少,其中Cs为MPPC的寄生电容,加上运放的寄生共模电容和差模电容。

参考附件关于跨阻运放的使用指南:
另外,MPPC不需要和运放的输入端之家串联电阻。