Other Parts Discussed in Thread: THS3091
在做宽带直流放大器末级功放的时候,我选择的是THS3091并联输出,然而前三级放大输出稳定波形,只要连接THS3091就会输出失真,但不是自激震荡(观察到的频率和信号输入的频率相同),请教各位这是什么问题引起的不稳定,怎么解决?首先可以确定的是不是因为相移引起的不稳定,因为测过输入信号和输出信号基本没有相位差;其次THS3091我是按照手册选的反馈电阻,十倍放大。TINA仿真图见附件。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的输出幅值是多少,我们实测在高频30MHz,输出幅值超过17Vpp时,才开始略有失真。
看你的应用,好像阻抗匹配不好。请参考以下的应用手册
1. 查一下是不是输入输出匹配的问题。对于输入匹配,可以断开3091和前级,用万用表先量一下前级输出到地的电阻,然后调节3091到地的电阻,使得前端输入匹配。对于输出,可以试试50欧姆匹配可不可以。
2. 你要推很大电流么?大电流输出或者高摆幅输出下,非线性会很严重,你试试只用一个3091,增益不放很高的时候,会不会有改善。
3. 输入信号频率很高的时候非线性也差,试试降频有没有改善。如果有改善,则需要设法展宽整条链路的带宽。
如果输出端负载就是确定的50欧姆,那么从输出端往里面看,应该看到一个交流50欧姆的电阻,用来和输出负载匹配。你可以试试在输出端接上50欧姆负载,然后调3091那两个电阻(95欧姆和866欧姆那两个)阻值,使得等效的输出电阻和负载匹配,看看会不会有改善。
上传一下你的电路图或者TINA文件以方便分析。
同时,如手册第一页左下角图示,当输出电压20Vpp时,THD在10MHz处只能达到-50dBc左右的水平。如果此时再增加摆幅,THD会更差。
输出波形是什么样子的?可以发上来看看。另外,匹配不是说在输出端接个50欧姆就可以的。你要么就调那个负载电阻让它和系统的输出阻抗相等,要么就按照手册第一页右下角图示,在每个3091输出端加上一个50欧姆电阻,然后在系统输出端接上一个到地的50欧姆。
系统输出阻抗是指从三个3091的输出往里看,看到的阻抗,这个阻抗如果是60欧,则在输出端应该60欧匹配;如果是100欧,就在输出端接100欧匹配。
Decapton Wang 你好,对于“那么从输出端往里面看,应该看到一个交流50欧姆的电阻,用来和输出负载匹配”这句话不是很理解,他所说的50欧姆负载应该就是一个电阻吧,为什么还要进行50欧姆匹配呢?不是在驱动特性阻抗是50欧姆的同轴线之类的情况下才要进行50欧姆匹配吗
你们是在做09年竞赛题吧,THS3091并联注意几个问题
1.并联后的输入阻抗是50Ω,与前级匹配
2.并联输出端不能直接接在一起,需要使用均流电阻
3.发热是必然的,需要设计良好的散热器,要不然是带不动50Ω负载的。
4.芯片的去耦和非常的重要