Other Parts Discussed in Thread: VCA810
我再用VCA810做压控放大时,当Vc调到-1.45左右时就出现了自激的现象。Vc从-1.0变到-1.4的过程还好,但是一超过-1.45(左右)就自激了。在社区上看过一些别的帖子,说是可能是因为在Vc等于-1.5时芯片的固有噪声滚降导致的。我也尝试将Vc调到-1.65左右,可还是自激了(输入为25mVp-p,500KHz)。请问专家,这是什么原因导致的呢。
附上原理图和PCB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,前面的线性可以是吗? 请先去掉C3试一试
有兴趣也可以和下面帖子的作者交流一下,因为他的问题刚刚解决不久。
http://www.deyisupport.com/question_answer/analog/amplifiers/f/52/t/25402.aspx
手册第三页,输入阻抗很大,可以视为高阻,这种情况下还需要输入匹配?你的信号源是50欧姆特征阻抗?如果不是,把R4去掉。
你的控制电压Vcontrol是从哪里来的?把C3换成个几百欧姆或者几K欧姆的电阻会不会有改善?
Layout可以参考手册22页Board Layout部分。
尝试过去掉Vc端的对地电容,没什么用。
看了那个楼主的帖子,出现的问题好像和我的不太一样。
反正我的电路要求在-20dB到+20dB正常工作就行了,现在差不多已经达到要求了。具体的优化过两天再做吧,这两天先把前级放大做了。
谢谢楼上两位专家的解答