This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问OPA2188的电压时多少伏?可不可以当做功率放大器?能否用在交流电路中?
单电源或者双电源可在+4.0V 至+36V(±2V 至±18V)的范围内使用。
不用于做功率放大器
可以在交流电路中使用
带宽2MHz
你可以参考OPA2188的datasheet
麻烦您可不可以给我推荐一款功放呢?电压在36V,用在交流电路中
请说的详细一些,具体的参数要求。
电压36V是什么?供电范围还是信号幅值?有效值?
负载是多少?