Other Parts Discussed in Thread: OPA698, VCA810
如上图(pdf15页,figure36),调控810增益的698的电源(即,正端+0.5v,负端-3.5v)为什么一定要这样供电?
我想,可不可以前级有一个运放做跟随器,然后,跟随器的输出短借个滑变调控,再接入810的3端?
还有,请教如果是前级接个跟随器,请问怎么防止电路自激振荡呢?
我是新人一枚,不知问的问题是不是有点太……还请各位大神指点。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
正电源小负电源大,可能是保证控制电压那条链路的输出(即810 VC脚看到的电压)能够小于0V。
跟随器加滑动变阻器的方法理论上可行,不过最好在调试的时候先用稳压电源供,把810调通了再换跟随器。
810需要输入匹配,如果前级是个跟随器,你可以在跟随器和810之间串一个电阻R,然后在810输入端到地接一个50欧姆,R的取值可能需要调整一下,最高50欧姆,往下调。
你好,
首先那个 +0.5V,-3.4V并不是运放opa698的供电电压,而是电压限制器的Vh与Vl,
opa698是电压限幅放大器,在两个电压限制端分别接入+0.5V -3.4V还是为了保证接入到VCA810的Vc端的电压时负值。
再次,你在前级接入电压跟随器不一定会引起自己震荡。如果在实际电路中出现了自激,就需要在级进行阻抗匹配了,很常用的就是串电阻(多数时候为50欧姆),接着同样的电阻接入地,后级级联VCA810。不过,这样的话,会牺牲掉你原来的增益,变为原来增益的一半了。
还有的办法便是在你输出端串联一个小电阻,也可以起到一定得作用,电阻值需要实际匹配。