Other Parts Discussed in Thread: INA333
为什么INA333单电源供电的时候REF需要接VCC/2,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于INA333自身来说是没有这个要求的。
你看到的在REF脚上加Vcc/2电压应该是和你的应用有关,比方你后端的ADC输入范围有关。
加Vcc/2,相当于把输出加了偏置,可以保证输出以Vcc/2为中心,上下摆动到0和Vcc,这样可以最大程度的使用ADC的全范围输入。
其实,可以把负电源端看成一个“地”。
1、如果负电源端接地,那么INA333输出的电压信号摆幅是以地为中心的,也就是说0V上下对称波形(不考虑直流成分)
2、如果负电源接入VCC/2,那么就相当于把上面的地抬高到VCC/2,此时INA333输出的电压信号摆幅是以新的“地”(即VCC/2)为中心的。
所以负电源端该怎么接还是取决于你的应用,看你设计的要求其输出摆动是怎样的范围,怎样的要求。