Other Parts Discussed in Thread: OPA4188,
仿真原理图如下附件,
1.仿真使用的芯片是OPA4277UA,实际焊接的芯片是OPA4140和OPA4188
2.OPA4140的测试数据如下。输入和输出在1.8V以内的线性度都是ok的,1.8V以上输出由偏差,随着输入电压越来越大,输出偏差越来越大(输入源:直流信号源)
序号 | in/输入 | out/输出 |
1 | 1.0V | 1.0V |
2 | 1.2V | 1.2V |
3 | 1.4V | 1.4V |
4 | 1.6V | 1.6V |
5 | 1.8V | 1.8V |
6 | 1.9V | 1.85V |
7 | 2.0V | 1.96V |
8 | 2.1V | 1.97V |
9 | 2.2V | 1.98V |
10 | 2.3V | 2.0V |
11 | 2.4V | 2.02V |
12 | 2.5V | 2.05V |
3.OPA4188对比测试,线性度非常ok