This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问专家有没有输出电压振幅大于10V正弦波的运放?

Other Parts Discussed in Thread: THS3001, THS3091, THS3120, BUF634, OPA228, OPA2134, OPA227, NE5532, OPA548, OPA541, OPA132, OPA211

请问专家有没有输出电压振幅大于10V正弦波的运放?

  • 能输出幅度大于10V正弦波的运放很多啊。重点在于你正弦波的频率多高?

  • 哦哦,我的正弦波频率在100HZ至40Khz之间,请问我手头上有个电流反馈型ths3001运用在音频会不会效果不好

  • 建议你看看THS3001技术手册

  • 你好,

    1、输出信号比较大,建议你注意下运放的压摆率的选择。

    2、THS3001输出电流150mA,用在电路最后一级做功放是可以的,具体效果如何要看你的设计要求

    3、对于这种功放级的芯片,给你推荐几个。THS3120,THS3091/3092,BUF634等,当然也可以采用晶体管扩流。

  • ths3001是一款高速运放,此外它是电流反馈型的  一般应用与高频

    楼主的主要频率在于100HZ至40Khz

    作为普通放大的运放推荐NE5532,OPA2134,OPA228,OPA227等

    作为最后功率输出可以考虑OPA548,OPA541等OPA5XX系列

    也可以考虑TPA系列的音频功率输出芯片

  • 我同意Shelher的观点。您的信号最大40kHz,幅度为正负10V,那么可以计算出您所需要的压摆率大约为2.5V/us,这个值很多普通放大器就可以达到,例如OPA132,如果增益较大可以用OPA211,等等。选择放大器时并不是速度越快越好,高速的放大器功耗很大,必要时还要设计散热,失调电压也很大,另外由于带宽很宽,其带内的噪声会较大,而且很容易自激震荡,特别是电流反馈型的放大器。因此设计时选择合适的放大器最好。