Other Parts Discussed in Thread: OPA330
参考电压VREF使用电阻分压设置的话应该怎么计算这里的电阻呢?A3下面的50Ω可以视作和R2并联吗?有文献说需要内置驱动器才能直接使用电阻分压,有推荐的型号吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本来内部运放A3的四个电阻都是50KΩ,其增益为1,如果REF pin外接电阻网络,那么等效电路相当于在右下角的50KΩ又串联了一个电阻,这个电阻值应该为R1//R2,使得A3不再对称或不再匹配,对共模信号的抑制能力大大降低,其增益也不再是1,A3的失调电流会被放大到输出。
应该怎么计算VREF
只要使用电阻网络生成VREF,那么就是电阻分压的方式计算VREF,即VREF=V*R2/(R1+R2)
但是不管怎样选择R1和R2,对右下角的50KΩ总会引入一个串联电阻,这个串联电阻会打破运放内部A3的平衡,或者说不再匹配。
R1和R2可以选小一些,对A3影响小一些但是电源V功耗就会大一些,总的是V功耗和A3平衡两方面的考虑。