Part Number: OP07


仿真了差分运放做的恒流源,但是整个电路不正常,图一是不正常情况下的图,虚短虚断不符合要求;图二正常,只是改变了运放的供电电压,有人可以帮忙解释下吗?感觉5V供电不是负反馈了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OP07


仿真了差分运放做的恒流源,但是整个电路不正常,图一是不正常情况下的图,虚短虚断不符合要求;图二正常,只是改变了运放的供电电压,有人可以帮忙解释下吗?感觉5V供电不是负反馈了?
您好,那是因为输入输出电压范围不在OP07的线性范围内,您看下数据手册的输入共模电压Vicm和Vout的电压范围,这是+-15V供电时的范围,可以看到输入范围为+-13V~+-14V, 因此+-5V供电的话,范围为+-3V~+-4V。输出也是,+-5V供电的话,输出范围典型值为+-3V。

所以通过您的测试可以看到,虽然输入测下来最高2.5V在它的输入共模电压范围内,输出恰好在2.99V,也就是3V左右,所以我认为+-5V供电没有给这个电路足够的阈值,所以导致运放不能更好的工作在线性范围内,所以通过提高供电电压的方法,使得它有足够的余量,不用+-10V,应该+-7V就可以使得它能正常工作了。